Change Language :
Choosing the right material for ball bearings is not always easy. In this article, you will find a brief summary of whether and when ball bearings made of metal, plastic or ceramic are suitable.
Metal ball bearings are mainly used in most classic mechanical engineering applications. They are number one in terms of global sales volumes and are suitable for a wide range of different mechanical engineering applications. However, they always reach the limits of their application when, in addition to load bearing and speed, further requirements are placed on the bearing. This applies, for example, to various sectors such as the food industry or medical technology. Here, specifications such as suitability for contact with food or suitability for use in cleanrooms are crucial. System manufacturers often require food certification in accordance with EU standard 10/2011 or FDA (American authority: Food and Drug Administration).
The advantage of plastic lies in the variety of materials. This means that different base polymers can be selected for a wide variety of applications, which are precisely suited to the application in terms of their specifications. In recent years, base polymers such as POM, PP, PEEK and other plastics have become established. Ball bearings made of plastic can be suitable for the following industries and applications:

In addition to the fact that xiros plastic ball bearings are corrosion-free and heat-resistant, they can also be used in chemical environments. Maintenance costs for plant and machinery can be reduced and reliability increased. The plastic ball bearings are characterised by low-friction dry operation, which means that xiros ball bearings do not require lubrication. This minimises rolling resistance. The reason: the balls do not have to overcome the resistance of the lubricant so that they can start up with a low breakaway torque.
However, plastic ball bearings can also reach their limits. For example, speeds in excess of 5,000 revolutions per minute can only be realised for a short time, as plastic deforms more quickly than metals at higher speeds and the resulting heat development. Bearings made of metal, on the other hand, have the edge when it comes to higher speeds and absorbing higher loads. This is where the metal variant scores points thanks to its combination of hardness and flexibility.
Yes, metal ball bearings are ahead in these disciplines, but the evolution of ball bearing technology is allowing the cards to be reshuffled. What exactly does this mean? igus® has always conducted basic research and a test laboratory that carries out around 135 trillion test cycles every year. In addition to investigations into friction coefficients and wear rates, corrosion behaviour is also on the agenda, for example.

Metal, plastic and ceramic ball bearings
For plastics and ceramics, aqueous media act like lubricants. With a suitable design, the coefficient of friction can be stabilised at a low level of around 0.1 or even lower. Wear is very low, so that a very long service life is generally achieved. In terms of load-bearing capacity and achievable speed, both plastics and ceramics have disadvantages compared to metals. Regardless of the variety of metal materials, metals have a good combination of hardness and flexibility. Plastic, on the other hand, is significantly softer and can deform more quickly (especially at high temperatures). Although ceramics are very hard, they also have the lowest flexibility and can break quickly under impact loads. In addition, the heat dissipation of ceramics and plastic is lower than that of metal. They are therefore also limited in terms of the maximum realisable speed.
In person:
Monday to Friday from 7 am - 8 pm.
Saturdays from 8 am- 12 pm.
Online:
24h
WhatsApp-Service:
Montag – Freitag: 8 – 16 Uhr